CRX-10iA/L Paint Painting an Electric Panel Box

How Collaborative Robotics Are Reshaping Modern Coating Operations

Paint cobots bring accessible, flexible automation to high‑mix finishing, simplifying programming while improving consistency, quality, and uptime.
Published
Reading Time
3 min
Share Facebook X LinkedIn Email

For years, collaborative robots have steadily made their way into welding bays, machine‑tending stations and material‑handling lines. Yet one area of manufacturing has remained stubbornly difficult to automate: finishing and coating. High‑mix paint shops have long struggled with the complexity and programming demands of traditional industrial robots. The arrival of paint cobots marks a meaningful shift in what’s possible.

Bringing a new level of accessibility to an industry that has historically required deep automation expertise, cobots are designed for manufacturers who need precision and consistency but can’t afford long programming cycles or specialized staff. 

Traditional paint robots often require point‑to‑point programming or offline tools that slow down changeovers. Yet a cobot can naturally fit into the rhythm of a high‑mix, low‑volume operation. Operators can guide it by hand to teach positions, drag and drop icons on a tablet interface, or simply press “record” and let the cobot capture an entire motion path in real time. For many shops, this means a new part can be programmed the same day it arrives, without waiting for a specialist.

The cobot’s capabilities extend well beyond ease of use. With large payload capabilities and extended reach can make it suitable for a wide range of coating applications, from liquid paint to powder and fiberglass. A cobot can handle virtually any type of spray gun with confidence and integrates cleanly with existing liquid or powder systems. Because it’s designed to work safely alongside people, a cobot can operate in tighter spaces and adapt to workflows that would be impractical for a traditional robot.

With simple integration of 2D and 3D vision part location systems, quality inspection is an area where paint cobots are quietly changing expectations. Tasks that once required separate manual checks, such as color and film (wet or dry) thickness measurement, surface quality measurement and defect detection can all be automated with minimal set-up and/or facility modification. With its low weight and 110 V/Single Phase power requirement, the cobot can be mounted on a cart, making it a flexible resource that can be moved wherever it’s needed – a very practical advantage, saving valuable area on a shop floor.

The broader story here is about accessibility. Automation in finishing has traditionally been reserved for high‑volume manufacturers with the resources to manage complex systems. Paint cobots lower that barrier, as well as the cost of adopting robotic equipment. They give first‑time automation users a tool they can learn quickly, trust daily, and adapt to a wide range of coating and inspection tasks. In an industry where labor shortages, quality demands and production variability are constant pressures, accessibility is more than a convenience — it’s a competitive advantage.

As the first cobot approved in North America for use in a painting environment, FANUC’s CRX‑10iA/L Paint is an ideal solution for manufacturers automating coating applications for the first time. Because it’s part of FANUC’s CRX series, it carries the same promise of eight years of zero maintenance, a rare level of reliability in environments where uptime is everything.

To learn more about how the FANUC CRX Paint Cobot can transform your operations, please fill out the contact form below. 

Ready to schedule a CRX Cobot demo or request a quote?
Let's Connect
Person Using CRX Programming Technology